Technical FAQs

Ask a Question

What thermal units are used in a 8940 Type SS* pump panels?

These controllers are provided with Solid State overload relays which are provided with an adjustable dial for selecting the thermal protection level.

CTA-ID : 2012619
Was this helpful?
What can we do to improve the information ?