Technical FAQs

Ask a Question

Can a single outdoor N3R HVL/cc switch section be ordered?

Yes. Only if it is 29.50`` wide. The smallest outdoor HVL/cc section is 29.50`` wide. This is dictated by the base channel, roof and outer door.

CTA-ID : 2012615
Was this helpful?
What can we do to improve the information ?