Technical FAQs

Ask a Question

Which CT should be used with HVL/cc?

Issue:
Which CT should be used with HVL/cc?

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Use the 3 phase (3 in 1) current transformer for HVL/cc when ever possible. This CT was designed and moulded to fit on the loadside of the HVL/cc switch bottle. Window type (donut) CTs will reguire separate incoming conduits due to the limited cable termination distance in the HVL/cc section.

Bar type CTs are not available in HVL/cc switchgear.


CTA-ID : 2012614
Was this helpful?
What can we do to improve the information ?