Technical FAQs

Ask a Question

Are the dimensions on the EZML333225 the same as they were on the EZML333200?

The dimensions are the same.


CTA-ID : 2012613
Was this helpful?
What can we do to improve the information ?