Technical FAQs

Ask a Question

Is there a design for the 38kV 150kV BIL HVL switch with bus penetration barriers and porcelain inserts? This is to prevent fault materials from propogating through the switchgear lineup.

At this time, there is no design at this voltage. Possibly some design could be done using 27kV MetalClad inserts. This would have to be entered as a Design Project in Development Engineering.


CTA-ID : 2012606
Was this helpful?
What can we do to improve the information ?