Technical FAQs

Ask a Question

Can R rated (Motor Fuses) be used in an HVL Switch?

Issue:
Can R rated (Motor Fuses) be used in an HVL Switch?

Product Line:
HVL.

Environment:
Products sold in the United States.

Cause:
Application.

Resolution:
Yes, R rated fuses can be used in an HVL switch as long and the dimensions are the same as our standard current limiting fuses.

Normally a 3`` diameter fuse.


CTA-ID : 2012605
Was this helpful?
What can we do to improve the information ?