Technical FAQs

Ask a Question

What is the acceptable wire size for a QO250GFI ?

Today each load lug is rated for 1 #12-#4 Al, or #14-#6 Cu. Older breakers used a lug that would only accept 1 #8-#4 Cu. Check the label on the breaker to verify the acceptable wire size.

CTA-ID : 2012378
Was this helpful?
What can we do to improve the information ?