Technical FAQs

Ask a Question

What is the speed regulation of the ATV11?

It is 0.5 x the motor`s nominal slip rating at base frequency for a speed range of 5% - 100% of base frequency, provided the motor`s nameplate values have been programmed into the drive`s drC menu.

CTA-ID : 2012365
Was this helpful?
What can we do to improve the information ?