Technical FAQs

Ask a Question

What is a RGC, RJC, RLC circuit breaker?

It is ``slang`` for a RG, RF, or RL breaker that is 100% rated. The ``C`` actually resides farther down in the catalog number just before the trip unit designation. The ``C`` denotes a 100% rating, not a connection type.


CTA-ID : 2012362
Was this helpful?
What can we do to improve the information ?