Technical FAQs

Ask a Question

Can the factory installed Q2M2200VH main breaker in the 300A or 400A CSED panels be upgraded to a 225 amp breaker?

Issue:
Application

Product Line:
CSED

Cause:
Application

Resolution:
The maximum amperage for the factory installed main breaker is 200A (ampere).


CTA-ID : 2012820
Was this helpful?
What can we do to improve the information ?