Technical FAQs

Ask a Question

Can HVL/cc be built 91`` deep to match the Masterclad?

Issue:
Can HVL/cc be built 91`` deep to match the Masterclad?

Product Line:
MasterClad.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Retrofit Job:
To build a 91`` deep HVL/cc to match Masterclad, a 53.75`` rear extersion would be required. The HVL/cc is only 37.35`` deep.
The best solution would be for the customer to use some conduit and come it the rear of the HVL/cc with a standard rear extension.


CTA-ID : 2012603
Was this helpful?
What can we do to improve the information ?