Technical FAQs

Ask a Question

How can a third cable per phase be added to an HVL/cc switch?

A third cable per phase will require an additional field shaper. The lugs must be bollted in the field shapers and a field shaper holds two lugs maximum.

Two fiield shapers require a 20`` wide section.


CTA-ID : 2012602
Was this helpful?
What can we do to improve the information ?