Technical FAQs

Ask a Question

Is Fuselogic (Indicaiton Only) available on the HVL 1200A 80kA switch?

Issue:
Is Fuselogic (Indicaiton Only) available on the HVL 1200A 80kA switch?

Product Line:
HVL.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No. The Fuselogic (Indicaiton Only) is not available on the HVL 1200A 80kA switch. The main blades have not been modified to accept the Fuselogic linkage. Also the back of the switch has extra bracing which will interfere.


CTA-ID : 2012601
Was this helpful?
What can we do to improve the information ?