Technical FAQs

Ask a Question

What are the number of operations of a Visi/Vac Circuit Interrupter?

The number of operations of a Visi/Vac Circuit Interrupter:

2500 full load operations 600 or 800A.
5000 no load mechanical operations.


CTA-ID : 2012600
Was this helpful?
What can we do to improve the information ?