Technical FAQs

Ask a Question

Can we offer 2000A or 3000A bus in HVL/cc. Indoor and Outdoor.

Issue:
Can we offer 2000A or 3000A bus in HVL/cc.  Indoor and Outdoor.

Product Line:
HVLcc

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
NO. 2000A and 3000A bus are not available for HVL/cc


CTA-ID : 2012599
Was this helpful?
What can we do to improve the information ?