Technical FAQs

Ask a Question

What are the best current transformers to use with HVL/cc switchgear?<br /><br />

The best current transformers to use with HVL/cc switchgear are the 3 phase CT`s which can be mounted on the load side of the switch.
This CT was moulded and designed to fit on the switch bottle.

Bar type CTs are not allowed.

Window type CTs require separate incoming conduits.


CTA-ID : 2012595
Was this helpful?
What can we do to improve the information ?