Technical FAQs

Ask a Question

How can the connecton from MetalClad main bus to HVL/cc main bus be selected in the Medium Voltage Metal Enclosed Product Selector?

Issue:
How can the connecton from MetalClad main bus to HVL/cc main bus be selected in the Medium Voltage Metal Enclosed Product Selector?

Product Line:
MasterClad.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
To select connecton from MetalClad main bus to HVL/cc main bus look in the Interrupter Screen and then the Lineside Connection drop down menu. Choose From MasterClad Switchgear.

The size of this transiton is under investigation. It has been built in a couple different dimensions.


CTA-ID : 2012594
Was this helpful?
What can we do to improve the information ?