Technical FAQs

Ask a Question

For HVL switchgear how can a PowerCast or Liquid Filled Transformer primary connection with RBA800 fuses be entered in the Medium Voltage Metal Enclosed Product Selector / Configurator? This applies to cable or bus connections.

There is not an engineering standard connection for this application.
In the product selector / configurator choose an outgoing 22`` terminal chamber and TAG in the applicable transformer connection charge. The 22`` transition section can be avoided by ordering a special transformer with high voltage terminals near the rear area of the switch. Caution, the extra engineering on the special transformer may exceed the cost of the transition section. Applications with space restrictions may require the special transformer.

CTA-ID : 2012593
Was this helpful?
What can we do to improve the information ?