Technical FAQs

Ask a Question

What is the difference between a QO2100 & QO2100H?

The QO2100H is rated for use on 3 phase corner grounded systems. They can be used in standard applications as well.


CTA-ID : 2012351
Was this helpful?
What can we do to improve the information ?