Technical FAQs

Ask a Question

What is the status of the XVA indicating banks?

The XVA units are obsolete. The new line of XVE products can be used to replace them. Lens units, bases, and support tubes are interchangeable. There are some parts, such as the standard flashing units, that have no direct replacement. The XVE`s have a lens unit with a integral flashing LED.


CTA-ID : 2012347
Was this helpful?
What can we do to improve the information ?