Technical FAQs

Ask a Question

Is there a motor cutoff switch on the front of the motor operated HVL/cc`s.

Yes.

There is a motor cutoff switch on the front of the motor operated HVL/cc`s. It also has a provision for a padlock.


CTA-ID : 2012583
Was this helpful?
What can we do to improve the information ?