Technical FAQs

Ask a Question

Customer needs the bolt that connects the breaker to the bus fingers on an EZM lineup.

The bolts are not field replaceable. Replacing would require disassembly....namely the insulating fiber that fits under the screw to protect it from the pan. The risk of damage to the fibers and difficulty of re-installation is too great.


CTA-ID : 2001904
Was this helpful?
What can we do to improve the information ?