Technical FAQs

Ask a Question

Can a ventilated transformer, enclosure style D, be ordered with the weathershield factory installed?

No, the weathershield kit is not available as factory installed. It would not be a value add to do so as the weathershield kit would have to be removed prior to removing the front cover for access to the terminal compartment (an extra step for the installer). Also, the weathershield would be too likely to suffer shipping damage in transit.


CTA-ID : 2012338
Was this helpful?
What can we do to improve the information ?