Technical FAQs

Ask a Question

What is the difference between RC200S and RC2M200S?

Issue:
Product Features

Product Line:
CSED

Cause:
Clarifying product features differences

Resolution:
The RC2M200S has provisions for a 200A max QOM2-VH and a 50A max QO-VH while the RC200S has provisions only for 200A max QOM2-VH.


CTA-ID : 2012332
Was this helpful?
What can we do to improve the information ?