Technical FAQs

Ask a Question

What size conductors does the QO116L125G neutral accept?

All terminals the minimum conductor is #14 CU and #12 Al
There is 1 neutral bar on right side. This has 3 holes with maximum 1/0 and 6 holes with a #6 max.
There are 2 neutral bars on left. One bar has 9 holes with # 4 max and another with 3 holes #4 max.
There is one large lug on one of these left side bars with range of 1 conductor #6 to 2/0


CTA-ID : 2012330
Was this helpful?
What can we do to improve the information ?