Technical FAQs

Ask a Question

Can a 3-Phase 4-Wire EZM meter center be fed from a 1-Phase, 3-Wire source?

No, from a product markings and UL Listing standpoint a 3-Phase EZM main (example: EZM3800CB) connected to a 3-Phase IN, 1-Phase OUT EZM branch unit (example: EZM314125) may not be installed on a 1-Phase, 3-Wire IN Service.


CTA-ID : 2035410
Was this helpful?
What can we do to improve the information ?