Technical FAQs

Ask a Question

What are the dimensions and weight for ATV28HU29M2U, ATV28HU18N4U, ATV28HU29N4U, ATV28HU18S6XU, ATV28HU29S6XU Altivar 28 drive?

Width = 5.118 in (130 mm) , Height = 5.906 in (150 mm), Depth = 5.906 in (150 mm)
The weight is 5.5 lbs (2.5 kg)

This information can be obtained in the ALTIVAR 28 Adjustable Speed Drive Controllers User`s Guide, Document Number: VVDED399062US



CTA-ID : 2012953
Was this helpful?
What can we do to improve the information ?