Technical FAQs

Ask a Question

How do you install the snap in mushroom on a 9001KR4/5 operator?

There is a tab on the mushroom that has to fit into a hole in the operator. Once you align this you have to push It very hard to snap it into place. It is a very tight fit so it will not come off once installed.


CTA-ID : 2035310
Was this helpful?
What can we do to improve the information ?