Technical FAQs

Ask a Question

What are the knockout sizes for the 8903LH**?

2 Power openings which will accept 1``, 1 1/4``, or 1 1/2`` hubs.
1 Control opening which will accept 1/2`` or 3/4`` hub.





CTA-ID : 2012798
Was this helpful?
What can we do to improve the information ?