Technical FAQs

Ask a Question

What factory modifications are available with a 9070 Type SK disconnect in the Mini enclosure? eg. 9070MN500G0D1

Transformer disconnects in Mini enclosures are limited to just one accessory, restricted to the E23 (electrostatically-shielded transformer), F11 (additional fusible secondary circuit), G13 (duplex receptacle, door mounted), or G14 (class A ground fault protected duplex receptacle, door mounted).

CTA-ID : 2012573
Was this helpful?
What can we do to improve the information ?