Technical FAQs

Ask a Question

Does the ATV58 unit have skip frequency capability?

Go to the SEt Adjust menu.
JPF, JP2 and JP3 can be set to jump frequencies. (Altivar 58 drives with less than V4.1 firmware only had one jump frequency.)
The drive will not run at the set frequency +/- 2.5 Hz.

CTA-ID : 2012329
Was this helpful?
What can we do to improve the information ?