Technical FAQs

Ask a Question

What is the wire range for a QOM 50 A breaker?

The lug for the lower amperage QOM breakers is the same as for the 100 A. Wire range is #12 to 2/0, torque is 50 lb. in.


CTA-ID : 2012317
Was this helpful?
What can we do to improve the information ?