Technical FAQs

Ask a Question

Can the Altistart ATS46 talk ethernet as a standard option?

The only communications protocols that are used are Modbus, Uni-Telway & JBUS. This requires part number VW3G46301U. It may be possible to get a third party bridge to convert Modbus to Ethernet.

One can go through Schneider Automation ( IAT Group) and they could offer a solution to talk Ethernet.

CTA-ID : 2012316
Was this helpful?
What can we do to improve the information ?