Technical FAQs

Ask a Question

How do I change the Altivar ATV66 unit from Keypad command to Terminal command?

Go to menu 5.0 and highlight Terminal command then press enter so that the dot shows beside this value.

To go to keypad command go to menu 5.0 and highlight Keypad Command then press enter so that the dot shows beside this value.

You can then set unit up to change between terminal and keyad by a logic input or function key.


CTA-ID : 7036
Was this helpful?
What can we do to improve the information ?