Technical FAQs

Ask a Question

When using the HarmCalc software, does it automatically include the reactance of the internal line reactor on the ATV58 units?

HarmCalc automatically includes the reactance value of the internal line reactors on the ATV58 units which have them built-in.

If there is additional impedance due to external line reactors or transformers this should be manually added to the calculations.

CTA-ID : 2012308
Was this helpful?
What can we do to improve the information ?