Technical FAQs

Ask a Question

What is the part number for the ATV56 keypad display?

The part # for the keypad is the same as for the ATV66, VW3A66206U.
All Altivar 56 drives are version 3.1 or greater. Therefore, it is not necessary to verify the revision level of the control board when replacing the keypad.

CTA-ID : 2012782
Was this helpful?
What can we do to improve the information ?