Technical FAQs

Ask a Question

Can we use a QOU breaker on 277v

No, the QOU breaker is rated for 120 Vac 1p and 240 Vac max 2 and 3 pole.


CTA-ID : 2012780
Was this helpful?
What can we do to improve the information ?