Technical FAQs

Ask a Question

What is the standard wire range of the DG/DJ/DL style breaker? Do they come with lugs?

When you order the D*L version of the breaker, the ``L`` in the catalog number means lugs come on both ends.
for 400 A breakers:
#2 AWG-600 kcmil stranded copper or #2 awg-500 kcmil aluminum

for 600 A breakers:
(2) #2/0 AWG-350 kcmil stranded copper or
(2) #2/0 AWG-500 kcmil stranded aluminum


CTA-ID : 2012541
Was this helpful?
What can we do to improve the information ?