Technical FAQs

Ask a Question

What is the operating temperature range of the XCDMP non contact safety interlocks?

The operating temperature range for that type of safety interlock is -13 to +185 degrees F, or -25 to +85 C.


CTA-ID : 2012528
Was this helpful?
What can we do to improve the information ?