Technical FAQs

Ask a Question

Is the MAL type circuit breaker made with trip free construction ?

Yes. Being trip-free is a requirement of UL 489 certification.


CTA-ID : 2012287
Was this helpful?
What can we do to improve the information ?