Technical FAQs

Ask a Question

What is the part number for ATV58 Digital I/O option card?

VW3A58202U.

This card provides 2 Logic Inputs, 1 Logic Output, 1 Analog Output, and A,A-,B,B- Logic Inputs for Encoder Speed Feedback.

This part number is listed in the instruction bulletin ATV58 TRX Installation Guide for Type H Controllers Bulletin No. VDVED397048US. This is available for download at www.squared.com


CTA-ID : 2012922
Was this helpful?
What can we do to improve the information ?