Technical FAQs

Ask a Question

Does the Altivar ATV58 drive have Analog Output?

ATV58 drives with control board versions 5.1 or greater include an analog output that can be configured for 4-20 mA or 0-20 mA. This revision was introduced in fall of 2002.

For ATV58 drives that have control boards with less than V 5.1 firmware, the basic controller does not Analog output.

Additional analog output(s) can be added with an I/O extension card.

CTA-ID : 6890
Was this helpful?
What can we do to improve the information ?