Technical FAQs

Ask a Question

Can an AFI breaker be used in a residence with a solar power system?

Yes, the AFI breaker will work with solar power. Some buzzing is considered normal when using an AFI breaker however it is more common when they are installed with solar power and non-sinusoidal current waveforms. It will not cause any problems with the operation of the breaker or the system.


CTA-ID : 2012921
Was this helpful?
What can we do to improve the information ?