Technical FAQs

Ask a Question

ATV28 using the remote keypad kit (VW3A28101). The remote keypad is showing ERR7. The keypad on the drive is OK. How can this be resolved?

Using the keypad that is on the drive, goto the I-O menu, and make sure the bdr (Serial Link Baud rate) setting is 19.2.
If it is at 9600, the keypad can not communicate.
If this does not resolve the issue, try another keypad or cable. Also, try this keypad and cable on another ATV28 drive.

CTA-ID : 2012916
Was this helpful?
What can we do to improve the information ?