Technical FAQs

Ask a Question

How do you enter a lineup in the product selector that is too long and will be split into 2 sections? This is an HVL lineup with Main-Tie-Main autotransfer and two Niagara Mohawk Meter Sections.<br />The sections will be connected with bus duct overhead.<br />

Do it as one lineup and TAG in the Bus Duct Connections on both halves and a bus transition section if required.


CTA-ID : 2011555
Was this helpful?
What can we do to improve the information ?