Technical FAQs

Ask a Question

How to key interlock HVL/cc lineup to other equipment.<br /><br /><br />Can the 600A HVL/cc switch withstand 700 amps for 3 minutes.

The small lock on the HVL/cc mechanism is only available from Schneider Canada.
For the keys to match the other equipment, the other locks need to be ordered from Schneider Canada. The dimensions are the same as Kirk Locks. The ones on the HVL/cc are different from Kirk and are much smaller and round.

The 700 amps for 3 minutes should be OK. This switch can carry 1200A with heat sinks.


CTA-ID : 2011554
Was this helpful?
What can we do to improve the information ?