Technical FAQs

Ask a Question

How do you pick the Fuselogic Options in the Product Selector?

When you pick FuseLogic in the Product Selector, it opens a menu of the versions of FuseLogic. EX:. Flag Only, Flag plus indicating contacts or Fuse Tripping.
I refer you to Product Literature on how the Stored Energy Mechanism operates.
Basically the close and trip springs are charged and waiting on a close or trip signal.
With FuseLogic, The pins on the fuses operate a shaft which is connected to the release latch on the trip springs.
When the fuse blows the mechanism will trip the switch.



CTA-ID : 2011552
Was this helpful?
What can we do to improve the information ?