Technical FAQs

Ask a Question

Can we have inner screen doors in a 5kV HVL switch section which is close coupled to an ATLAS transformer which will match Square D transformer terminals?

The current design does allow for screen doors with standard cable connections to Square D transformers.
Screen doors are not available for bus connections.

This job will be OK with a screen door in the switch connecting to the transformer with some special make parts.


CTA-ID : 2011548
Was this helpful?
What can we do to improve the information ?