Technical FAQs

Ask a Question

What fuses can be used for HVL Fuselogic indication only dry contacts.

Issue:
What fuses can be used for HVL Fuselogic indication only dry contacts.

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
For Fuselogic on HVL the Square D fuse designed by Ferraz Shawmut must be used. The maximum fuse sizes are 450E at 5kV and 200E at 15kV. This fuse has the extended travel pin and and stronger spring for the pin.


CTA-ID : 2011547
Was this helpful?
What can we do to improve the information ?