Technical FAQs

Ask a Question

Are parts still available for the ATV452 or 8803 Omegapak drives?

There are limited replacement parts available from the SquareD drives repair depot. Call Drives PSG to help identify replacement parts. They will contact the repair depot if necessary.
In some cases, it is more cost effective to replace the entire drive.
The product was discontinued in 1995.
Parts are no longer available from the manufacturer in France.
This announcement was made 07/2003

CTA-ID : 2012077
Was this helpful?
What can we do to improve the information ?